You are here: Tools > Human Machine Interface Editor > Design the HMI with the Internal Editor

Design the Control Panel with the Internal Control Panel Editor

This section details the Controls and Properties used to define the Control Panel when you need to debug your application, as well as the procedure for Mapping Variables to the Control Panel controls.

 

Create Control Panel

Use the Control Panel control library

Edit the Control Panel

Mapping Variables to the Control Panel

Graphic Objects

Graphic Objects Properties

Operate the Control Panel


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™